STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0RB Discovery Board

Hi, I am new to work on STM32F0 discovery board. I am Implementing the USB communication TX/RX with iMX8 controller. I am trying to send  and receive the 65 bytes of data packet, but it is communicating only 64 bytes of data packet, as its implemente...

Writing to a USB stick from STM32G474Cx MCU

I would like to preface with the fact that I am fairly new to hardware programming and electronics hardware design so bear with me if I am making some beginner mistakes.I am trying to write data to a USB stick using the PA11(33) pin and the PA12(34) ...

Resolved! USB DFU configuration / use

Hi,I used a F105RCT6 in a custom board, i want to use the DFU mod.When I generate the project with cubemx I select USB DEVICE and DFU mid, i change the clock configuration corectly. I generate the FW, and i flash him.The DFU is running, i open cubepr...

problem in the implementation of USBOTG

I am currently working on a project that involves integrating USB functionality for data transfer and data logging on an STM32F407VG micro-controller. Specifically, I want to log data files on an SD card and enable the user to download these logged f...

Resolved! How to configure abd read data with STWIN.box

Hello ,I recently bought the STWIN.box core system board (STEVAL-STWBXCS1), so I don't know everything about it. I would like to carry out a predictive maintenance project. I followed the steps below:1- flash the binary file with STM32CubeProgrammer2...

AkaPaDa_18_0-1694676545454.png AkaPaDa_18_1-1694676590371.png

Resolved! STM32F105 on board STM32F401 not working USB

Hello.I buy board STM32F401Development Board V3.0 STM32F401CCU6  .Board workin and work usb, but me need can bus.I replase  SMM32F401 MCU on STM32F105RCT6.Board work and programming bun not work USB ((. DFU mode not work.I searching difference USB be...

bithasher by Associate II
  • 566 Views
  • 12 replies
  • 1 kudos