STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Disabling GPIO Clocks for AF I/O Fails.

Posted on June 12, 2017 at 18:30The data sheet for the STM32L476xx (DocID025976 Rev 4 states on page 124, footnote 2 of table 40) states:� In order to save the full GPIOx current consumption, the GPIOx clock should be disabled in the RCC when all po...

STM32L475 Internal Flash driver write issue

Posted on May 09, 2017 at 15:02We are working on STM32L475 Internal Flash driver and we are facing one issue and to solve that issue i need below clarification.Is it possible to program any Flash location twice without erase?. lets say there is one ...

Resolved! another bit band question

Posted on February 20, 2017 at 20:08hey everyone,i was using stm32f103 and i was doing a bit-band on gpioa. Now i'm trying on cortex-m4 stm32L432 with no luck. Something changed in L4? Has onyone used bigbanding on gpioa @ stm32l4?thanks in advance#...

John Doe1 by Associate III
  • 236 Views
  • 7 replies
  • 0 kudos

NucleoL476RG and SD card using SPI issue

Posted on May 26, 2017 at 10:56HI Everybody,I am trying to access microSD card with NucleoL476RG board using SPI interface. I am using FatFs third party library with code (generated from stm32cubemx software). I did everything but it is not working....

Demo app already installed on STM32L476-DISCO

Posted on June 03, 2017 at 08:20Hello,I fiddled around with an stm32l476 discovery board. Is there a way to reinstall the demo app originally installed on the device? Is there a place where I could find the source code?Kind regards,aannoBtw, the boa...

Resolved! How do I get started with the B-L475E-IOT01A?

Posted on May 31, 2017 at 17:33How do I get started with the B-L475E-IOT01A?  I must be missing something?  I assumed there would be support for this board on mbed?  Are there any example projects?  I want to be able to test drive the various transp...

STM32L433 strange temperature sensor readings

Posted on May 30, 2017 at 08:50Actually I am working with a STM32L433CBY controller. When using the internal temperature sensor I got some inconsistencies and strange readings. Maybe someone can clarify the issues.1. Reference temperature TS_CAL2The...

STM32L432KC: which reference manual should I use ?

Posted on May 19, 2017 at 08:30Hello everyone,Can somebody please explain me what are the differences between RM0393 (which is specific to STM32L4x2, but latest release is from May 2016) and RM0394 (which is specific to STM32L43xxx and so on and lat...

Kraal by Senior III
  • 82 Views
  • 2 replies
  • 0 kudos