STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151VE ADC

"The ADC of STM32L151VE is not functioning properly. The output values of the ADC appear to be random. Does anyone know how to resolve this issue?

20230627145511809.jpg

Cleaning after reflow: STM32L151VC6 UFBGA100 package

Hallo, I have a question for the STM32L151 in the UFGBA100 package.There is a technical note  for the WLCSP-package existing (TN1163). In this note it is not recommended to clean the WLCSP package and also apply no ultrasonic cleaning methods.We are ...

geigerm by Associate
  • 158 Views
  • 0 replies
  • 0 kudos

Resolved! I2C does not work with Arduino IDE and STM32L152

Hi,I tried the following program:#include <Wire.h>   void setup() { Wire.begin(); //creates a Wire object // set I/O pins to outputs Wire.beginTransmission(0x20); // MCP 23008 Port Expander Wire.write(0x00); //selects the IODIRA register Wire.write(0...

PStol.1 by Associate
  • 213 Views
  • 3 replies
  • 0 kudos

STM32L1 NRND'd

One of my friends noticed, that ST NRND'd not only the STM8, but also the whole STM32L1xx family.However, in contrast to STM8, the 'L1 are under the 10-year commitment program, so they should continue to be available in the next 9 years. JW