STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hex file compatibility

Posted on July 19, 2013 at 19:46It's possible to create an hex file with IAR Embedded Workbench and download through the keil uVision the same file?I have an error:No Algorithm found for: 00000000H - 0000063FH #hex-file-stm32f103-iar-keil

STM32F103 Internal Flash Bank2 Access

Posted on May 31, 2013 at 13:57I am working on a project using an STM32F103 with 768K of internal Flash. I can successfully erase and program the first bank of internal Flash, but am having problems with bank2. The problem seems to be that I am havi...

stuart by Associate
  • 122 Views
  • 2 replies
  • 0 kudos

USB Device using SDHC through SPI in STM3210C-eval

Posted on July 02, 2013 at 22:09Hi,I am working in a USB Device project. The idea is plugging the device in the PC via USB cable in order to mount a drive unit. Data is storaged in a SD card through SPI interface. I am using STM3210C-Eval board and ...

gustavo2 by Associate II
  • 64 Views
  • 3 replies
  • 0 kudos

STM32F103 I2C EEPROM oddity

Posted on June 17, 2013 at 00:39I am trying to use the I2C to read and write to an external 24LC024 EEPROM.  I am using a polling method since my DMAs are being used for USART2.  I remapped I2C1 to PB8/PB9.  When I read the EEPROM it works fine and...

STM32F103 internal temperature sensor

Posted on June 11, 2013 at 14:12Hi! I have seen an earlier discussion with the device stm32F051 or F205 regarding the TS_CAL1 and 2 values. My question is, are these values applicable for the STM32F103 device? Cannot find any references to them in t...

peter23 by Associate II
  • 169 Views
  • 8 replies
  • 0 kudos

STM32F1xxx Clock Configuration Tool?

Posted on May 08, 2013 at 02:18Is there one?  I found the STM32L1xxx here http://www.st.com/web/en/catalog/tools/PF257838, but can't find one for the STM32F1xxx line.  Perhaps the L1 version will work for the F1, but I can't find any resource that i...

chogan by Associate
  • 64 Views
  • 1 replies
  • 0 kudos

Question about the RTC of STM32F103

Posted on May 07, 2013 at 15:29We're using RTC as a timer to wakeup STM32F103 from stop mode frequently, I'm quite confused on the descriptions in RM00081. what's the difference between RTC_IRQHandler and RTCAlarm_IRQHandler? If an alarm comes, both...

qinghui by Associate
  • 56 Views
  • 0 replies
  • 0 kudos