STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer OC Mode

Hi.I need help understanding how the timer works, because I'm faced with a situation that I can't understand.I use F091RC (board: nucleo)I created a new project in the CubeMX, timer 2 (CH1) configured in OC mode.Prescaler = 0ARR = 5000-1CCR1 = 2500-1...

f0_tim2_timnig_even.png f0_tim2_timnig_odd.png
Vch.1 by Associate II
  • 375 Views
  • 12 replies
  • 0 kudos

STM32F0 Discovery board

Hi,   I am new to work on STM32F0RB discovery board to get update the FW through UART/USB port. If any one have the idea to work on this please give me the solution.   Thanks, Shashi Shekhar

STM32F0RB Discovery Board

Hi, I am new to work on STM32F0 discovery board. I am Implementing the USB communication TX/RX with iMX8 controller. I am trying to send  and receive the 65 bytes of data packet, but it is communicating only 64 bytes of data packet, as its implemente...

How to use DMD P10 LED displays with STM32

Hi there,I am working on a project where I am using STM32F401RE but later might shift to STM32F0 controller for interfacing it with DMD P10 LED display (monochrome/RGB), so are there any resources available for that? By resources I mean, libraries an...

DJ17 by Associate II
  • 160 Views
  • 1 replies
  • 0 kudos

Resolved! Kit/boards recommendation for handheld game console

Hi,I have for dream to be able to create a handheld game console like the PSP when I was younger. It's for this main reason I study electronics.I wonder if there is a kit that help me to understand and learn about the concept of it or something not t...

KarlY by Associate II
  • 705 Views
  • 8 replies
  • 2 kudos

Resolved! Product life

Hello, We are looking for Controllers for our us based client. I want to know Product life and active years from this family of STM32(STM32F0 Series, STM32F4 Series, STM32F7 Series).  Can Someone help to find where i will get this info.it should be g...

Gajanan by Associate II
  • 112 Views
  • 3 replies
  • 0 kudos

Resolved! 4 cahannel PWM making (2 ch + complimentory )

Hai ,am trying to make a pwm signal to drive an H bridge driver  ,My board is Nucleo-F070RBI am using the following function HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1);HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1);HAL_TIM_PWM_Start_IT(&htim1, TIM_C...

Resolved! Problems with ST-LINK/V2

Hi,I recently bought a ST-LINK/V2 dongle and it didn't work. I checked the insides of it to see that the microcontroller inside wasn't an ST one, but a Geehy clone microcontroller. I bought another, which was not a dongle, it was the larger white ver...

JS8 by Associate II
  • 319 Views
  • 7 replies
  • 1 kudos