STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 + I2C

Posted on August 06, 2013 at 14:26Hi Guys,does anyone of you have a simple interrupt base example for a I2C communication with the STM32F0 using the FW-Lib from ST. I've found nothing in the net and I can'T use the examples of the STM32F1 because th...

manuel by Associate II
  • 47 Views
  • 1 replies
  • 0 kudos

Stm32 Encoder interface

Posted on July 12, 2011 at 11:20Nid help in Stm32 Encoder Interface, to turn the motor in clockwise and anti-clockwise direction. Thanks  #encoder-interface #stm32f0-discovery

STM32F051 IAP w/o a pushbutton

Posted on August 15, 2013 at 21:45Hi,We are developing a product using a STM32F051 and want to be able to upgrade the code using IAP. I've been reading anything I can find, AN4065, the examples, etc. It seems like the general idea is that the micro ...

munger by Associate II
  • 75 Views
  • 4 replies
  • 0 kudos

STM32F0 How to reset SPI interface?

Posted on August 15, 2013 at 16:36Hi, I've a problem with the SP interface. If I reset continously the uC (maybe interrupting the SPI communication would do the same) sometimes the receive buffer gets a 4-bit offset. I do communicate with 8-bit valu...

Is there STM32F051x8 in stop mode has a 1ms timer

Posted on August 05, 2013 at 09:43Hi,I am using the STM32F051x8,I want a timer which could interrupt every 1ms in the stop mode?But I have found the TIM can't work in the stop mode,and the RTC just happen interrupt every second. How can I do?Thanks?...

STM32F0 ADC DMA sample rate

Posted on July 25, 2013 at 08:40I need to setup the ADC -> DMA to transfer at exactly 44100 hz. (Audio quality)I have setup the DMA -> DAC by setting the clock to TIM_Period to 1088 (48Mhz / 1088 = 44117) But i dont seem to have this control over th...

justin by Associate II
  • 98 Views
  • 3 replies
  • 0 kudos

STM32F051C Alternate Function Register problem

Posted on June 28, 2013 at 11:12Hi Everyone! Sorry for interrupting all of you, but I have a problem. Next year I will graduate from my University as an Electrical Engineer (at least on paper I will be one). For my thesis I'm currently using an STM3...

MicroXplorer STM32F050 support

Posted on June 26, 2013 at 16:54Hello, when will the ''UFQFPN28''  package be supported by this tool? Currently I only see the 32 and 48pin packages supported.ThanksD #stm32f050g4-stm32f050g6-stm32f0

db91360 by Associate
  • 46 Views
  • 0 replies
  • 0 kudos