STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB CDC data loss

Hello,I am trying to transmit some data on my STM32F042F6P6. But my PC's serial monitor only picks up some of it. Here is the code and the serial monitor output:void readAllRegs(void){ uint8_t value; for (uint8_t addr = 0x00; addr <= 0x2E; addr++...

LLope.31 by Associate III
  • 1406 Views
  • 7 replies
  • 1 kudos

Resolved! What is USART CTS latency?

I am starting a product design tentatively using the STM32F072RBT6.I want to determine how soon the CTS input must go low to prevent the USART from transmitting the next byte.Even informed opinion would be appreciated; but a reference to documentatio...

usart clocks.jpg

Remote wakeup on STM32F0

Trying to implement a composite HID device on STM32F042 (or maybe STM32F072 as both Flash and RAM usage seem insane), starting from the MX mouse middleware. After much scratching around it's finally working as a mouse and keyboard and I now need to a...

NTC-Temperature Sensor

I used STM32F072C8T6.ADC - IN0, IN1 set.An application that measures temperature with an NTC temperature sensor.​   ​PullUp resistance 10K was connected to Vdd (3.29V) and PA0, PA1..When the HAL_ADC_Start_DMA function is executed, the voltage of ADC ...

스크린샷 2024-02-26 214841.png
hwm by Associate
  • 124 Views
  • 2 replies
  • 0 kudos

ADC differences at an STM32F071V8Tx

Hi, we use 12 ADC channels to measure temperatures in a smart home project. The system clock of the STM32F071V8Tx is configured at 48 MHz. Due to the slow temperature curve, we use the longest sampling time. We have taken a conversion table from a da...

albreco_0-1708966365820.png
albreco by Associate
  • 105 Views
  • 1 replies
  • 0 kudos

Resolved! TFT Screen Library in STM32CubeIDE.

Dear Experts,I have 4 inch RPI LCD 480x320 SPI based on the ILI9486 display driver. Like inside ArduinoIDE, there is a Library manager where we can find so many TFT-LCD libraries with STM32 board support, Is there a common place to find libraries for...

YashJ by Associate III
  • 133 Views
  • 4 replies
  • 0 kudos