STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm out before I even really got started...

Hopefully someone at STE cares enough to take this honest feedback on board...My project had to move from atmel to something with more performance.  I settled on STM32.The experience has been terrible due to sub-optimal documentation from STE, relyin...

Rust

Hello, I have a question for you, does the ST company have a program for the Rust language?

AHass.5 by Associate II
  • 487 Views
  • 5 replies
  • 0 kudos

USART Tx DMA on STM32H5

I'm using an STM32H563 and the STM32CubMX for initialisation. I'm trying to use the USART in DMA mode and having trouble with the Tx DMA.I use:HAL_UARTEx_ReceiveToIdle_DMA(&huart10, (uint8_t *) uart10RxDMABuffer, UART10_RX_BUFFER_SIZE);for the receiv...

Resolved! STM32H7 | MPUs in dual cores

Hello @ all,I'm dealing with a project with stm32H755 MCU, as you know it is made of two cores: cortex-M7 and cortex-M4. Keeping in mind I'm using a few peripherals, among which FDCAN, SPI and most importantly lwIP/ETH, I'm trying to put together all...

Zzaaack by Associate III
  • 899 Views
  • 3 replies
  • 3 kudos

Resolved! Maximum External Clock supported by stm32F767.

I looked at both the datasheet and Oscillators design document for stm32 controllers. Both suggested the same speed for external Osciallaotrs for stm32F7 controllers that is 4-26 MHz.BUT, in the stm32cubeMx it gives you option to select external HSE ...

CJami_0-1696839447346.png CJami_1-1696839455028.png CJami_2-1696839494005.png
CJami by Associate II
  • 485 Views
  • 4 replies
  • 3 kudos

How to calibrate RTC on STM32F411CEU6

Hello everyone! I have stm32f411ceu6 dev board, and I decided to use RTC. But it's going slower than time on reference clock. I use 32768 oscillator, which is soldered on the board. Can I calibrate this thing?