STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

standby and reset

Can't find a source file at "C:/Users/mmm/Documents/Projects/stm32 projects/AccessMini/Debug/../Core/Startup/startup_stm32c011f6px.s"Locate the file or edit the source lookup path to include its location. what does this statements?Anything to do with...

meena by Associate III
  • 160 Views
  • 0 replies
  • 0 kudos

Resolved! How to use ST32MC0 for I2C communication over 2050 bytes?

I am using STM32C031C6 for I2C verification.I tried to communicate 2050 bytes of data using the HAL driver.However, it did not receive the correct data.To be precise, the data at 512,1024,1344,1346,1538,18561 and 1858 bytes were different.The setting...

kkazu by Associate II
  • 563 Views
  • 4 replies
  • 1 kudos

stm32c011

please let me know my coding is correct ,whether usage of my exti is correct  while (1) { HAL_Delay(300); // MAINS INPUT Adc_Mains(); HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1,1000); Main...

SRAM.11 by Associate III
  • 226 Views
  • 0 replies
  • 0 kudos

Pwr_wakeup

I couldn't able wakeup the system after standby (wakeup should be switching ON mains ) the wakeup pin PA2 is connected to mains pin configured for pwr wakeup.  int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuratio...

SRAM.11 by Associate III
  • 261 Views
  • 2 replies
  • 0 kudos

low power modes

this part in my code completely making my prototype to sleep which should not.As my standby should workout if the main power supply is OFF for 30 seconds.I have tried shutdown mode and exti thats too behaved the samePlease help what may be wrong  _...

meena by Associate III
  • 185 Views
  • 0 replies
  • 0 kudos

Multi ADC READ

I am trying to read Analog voltage from two different channel one is mains supply and another is battery voltage.But I am getting both values same in live expression window.Does my config wong.Pls helpvoid ADC_Mains(void) { ADC_ChannelConfTypeDef s...

meena by Associate III
  • 204 Views
  • 1 replies
  • 0 kudos

stm32co debugger/programmer

Hi,I am using a prototype with stm32c011f6p6 MCU to program that Can i use STM32F40 discovery kit.I used but I couldn't able debug.I need to is it possible or I need to buy a separate programmer.any issues with hardware i couldn't able to find out.ca...

SRAM.11 by Associate III
  • 181 Views
  • 1 replies
  • 2 kudos