STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C011 unbale to configure nRST pin as GPIO

Hi everyone,Recently started working on STM32C011J4M3 micro. I'm trying to set PF2-NRST pin as a GPIO. but when I configure it from cube MX as GPIO PIN always reamins in High state that is a 3.28v and i'm unable to toggle the pin or perform any other...

STM32 Technical Updates are back : 2024 Newsletter 1 !

Dear STM32 users and developers, This new thread is back and is dedicated for our technical developers community to share last STM32 updates, the first part will be products documentation news such as datasheets, Erratas, Applications notes  followed...

STM32 Technical updates - 2024 Newsletter1.png
STOne-32 by ST Employee
  • 376 Views
  • 4 replies
  • 13 kudos

Resolved! Flash endurance parameter

Hi,Can somebody please explain what the "Flash memory endurance" value in the datasheet means? The max number of overall writes to the flash page or the max number of writes in the particular "cell" inside the page?Simple context:Let's say that the M...

kvrbek by Associate II
  • 81 Views
  • 2 replies
  • 1 kudos

Resolved! Avalonia UI?

Hi All - Not sure if this is the right place to ask this, but thought I would try anyway.I just finished a project that used Avalonia UI (C# based cross platform system for application GUIs) on a raspberry-pi 4 with a Waveshare touch screen attached....

clawton by Associate
  • 103 Views
  • 2 replies
  • 0 kudos

Resolved! STM32C0 bootloader UART pin assignment

Hello,I have a question regarding the bootloader of the STM32C0 (especially the TSSOP 20 version STM32C031F6Px).According to the datasheet and the reference manual, the bootloader can communicate via UART1 and I2C1.The pins it is using are PA9&PA10. ...

akurtj by Associate
  • 114 Views
  • 2 replies
  • 1 kudos

Resolved! ADC input resistance STM32C011J4M6

Hi everyone,I am using the STM32C011J4M6 in the SO8N package.I want to use the ADC on a low frequency signal (around 1kHz). My application needs to be very low power so I decided to put a big (around 100kOhms) input resistance on the ADC pin like we ...

Pierre75_0-1706438661717.png Pierre75_1-1706438870749.png
Pierre75 by Associate II
  • 236 Views
  • 7 replies
  • 3 kudos

Resolved! STM32C011J4M6 conflict on pin

Hello everyone,I have a question about the STM32C011J4M6 in S08N package.I am developping a PCB with this MCU and want to use an LSE like in the picture below.Then I also want to program and debug my MCU with an stlinkv3 and will use the SWD debug so...

Pierre75_0-1705586401952.png Pierre75_1-1705586566297.png
Pierre75 by Associate II
  • 288 Views
  • 6 replies
  • 0 kudos

Resolved! STM32C0 SO8N bootloader: I2C and SWD

Hello,which interfaces does a virgin STM32C0 in SO8N offer on the first boot for programming? AN2606 says USART1 and I2C1. In other cases, AN2606 adds a note when SWD does not work, but no such note is there for STM32C0. So, I assume SWD is supported...

lukasl by Associate
  • 187 Views
  • 2 replies
  • 3 kudos