STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Differential Mode SDADC Codes

Posted on May 26, 2016 at 04:57I need to know what the differential mode SDADC conversion code is. Is it 2's compliment such that the code:  int16_t D = (int16_t)HAL_SDADC_GetValue(&hsdadc3); Will return to D a signed result such that if the positiv...

spflanze by Associate II
  • 244 Views
  • 3 replies
  • 0 kudos

STM32F373 sdadc linearity at low input drops off

Posted on March 20, 2016 at 18:07With a 'F373 I find that the sdadc counts-per-volt of the SDADC drops off rather dramatically when the input voltage decreases below about 40% of FS.  I would like to understand the mechanism behind this before locki...

Configuring SDADC and ADC Repeat Triggering With DMA

Posted on January 16, 2016 at 07:06I am triggering ADC1 from TIM4->CCR4 and SDADC1 from TIM4->CCR1. ADC1 is configured for regular conversions and no injected conversions. SDADC1 is configured for injected conversions and no regular conversions. For...

spflanze by Associate II
  • 128 Views
  • 2 replies
  • 0 kudos

SDADC Gain 0.5 max Vin?

Posted on December 08, 2015 at 22:02Hi, According to AN4207 page 10, in Single ended zero ref mode the max input voltage to the ADC is Vref/gain. So if I set Vref = 3.3V = VCC, can I measure up to 6.6V with gain = 0.5? Or would this collide with the...

0690X0000060361QAA.jpg

STM32F373 SDADC (Sigma-Delta ADC)

Posted on March 18, 2014 at 03:12Hello, I am planning on using the SDADC in STM32F37x microcontroller.  The data sheets says the sampling frequency is between 500 kHz ~ 6 MHz, depending on the clock signal driving the SDADC.  The output data rate is...

jim_wei by Associate II
  • 212 Views
  • 4 replies
  • 0 kudos

SDADC Manual code Examples

Posted on March 23, 2015 at 18:03Good Day,Could anyone please help?i am Currently developing using a STM32F373 MCU and Struggling to get the SDADC Working According to the Reference manualI am using the MikroC Compiler and there are no SDADC Librari...

jody by Associate
  • 242 Views
  • 2 replies
  • 0 kudos

SDADC2 synchronization with SDADC1

Posted on November 26, 2014 at 10:43I have seen a lost of discussions about synchronized sampling of ADCs. But I haven't seen a single example for synchronized sampling of SDADCs anywhere. I am using stm32f373 MCU where I want to sample SDADC1 and S...

rizwin by Associate II
  • 124 Views
  • 2 replies
  • 0 kudos