STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NAND memory read errors

Posted on January 11, 2014 at 23:08Hello,I will try with this forum as a last resort for my problem, namely getting my NAND memory to play with me.http://www.ic-on-line.cn/download.php?id=1915099&pdfid=5E619D21E0C125A4A94BC1A860068896&file=0459\h27u...

STM32F4Discovery (FSMC) + FT2232H

Posted on September 12, 2013 at 04:07 Hello, I have paired up an STM32F4Discovery board with an FT2232H part from FTDI. The purpose of this is to use the CPU-FIFO mode of the FTDI part for faster USB data transfer. I made the necessary mo...

mehmoodn by Associate
  • 246 Views
  • 1 replies
  • 0 kudos

STM32F103VG FSMC/LCD

Posted on December 17, 2013 at 19:27Dear Sirs I developed a system with a STM32F103VG  processor. The processor is connected to an LCD with Intel 8080 interface. I use FSMC to configure and manage the LCD. The processor is configured to run at 72MHz...

STM32F4 Discovery FSMC not working in 8bit mode

Posted on July 15, 2013 at 21:40 Hello I am working on a project that uses FSMC .Everything is fine when I use 16bit mode but in every write i need to shift the data <<8 to bring it on to the D8-D15 lines . I cant use DMA like this . so i need a...

stm32f427 fmc or fsmc?

Posted on December 02, 2013 at 12:58Hi,I'm programming a STM32F427, so I'm searching between datasheet and libraries. I don't find answers anywhere, I don't understand if STM32F427 supports a flexible memory controller (FMC) or a static one (FSMC), ...

stefy_tp by Associate II
  • 390 Views
  • 5 replies
  • 0 kudos

TFT LCD with FSMC and External RAM

Posted on June 14, 2012 at 10:00Hi all,I'm working on a project with a dumb TFT LCD (320 x 240). I'm trying to display static images (no double buffer). I've been able to display images (in 565 format) that I load on the flash memory and refresh it ...

joembiye by Associate II
  • 545 Views
  • 10 replies
  • 0 kudos

Addressing 16-bit variables 512K SRAM

Posted on September 04, 2013 at 13:05Hi everyone. I can't get my head around this ... I was using a SRAM memory of 128K in a project, interfaced via the FSMC controller, but now I have to extend it to 512K. I have 16-bit words to store in the memory...