STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EEPROM emulation hard fault

We have another problem with EEPROM emulation. We use STM32H723Z and store user configuration to flash as emulated EEPROM. I used driver from the H7 examples' directory as a basis.When we write the configuration heavily, after few days, there occurrs...

Resolved! EEPROM emulation on STM32H7

This issue was already mentioned here except now it is on different line. I think it is still there.In EEPROM emulation in the \STM32Cube\Repository\STM32Cube_FW_H7_V1.9.0\Projects\STM32H743I-EVAL\Applications\EEPROM\EEPROM_Emulation\Src\eeprom.c fil...

Push Button with EEPROM via I2C and LCD

I am a beginner in STM 32 and working on a Temperature controller where I have 4 Input push buttons to change the set parameter and store in EEPROM via I2c, pls help to resolve the issue where I am stuck, if you can guide me on free/paid basis, will ...

VSing.4 by Associate
  • 112 Views
  • 1 replies
  • 0 kudos

eeprom write page error

Hi,I am trying to write some datato external eeprom with I2C_EEPROM_WritePage function, but it doesn't write everytime. Sometimes it can write and sometimes it can't. I am using standart peripheral I2C library and using the write page function below....

er3481 by Associate III
  • 102 Views
  • 0 replies
  • 0 kudos