STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to Generate the Clock for EXTI ?

Posted on July 06, 2018 at 16:09Sorry for my stupid question, but this makes me really confused. I was just looking for the the bus with connected with the EXTI, then I found that APB2 bus is connected as it is shown in the reference manual in here ...

Error in the STM32F745 datasheet

Posted on April 23, 2018 at 09:19Hello,I found a error in the STM32F745 datasheet (DocID027590 Rev 4).In table 24 on page 222 a pitch of 0.5 mm is given for the UFBGA176 - 10 � 10 mm package.In table 120 on page 216 and 217 a pitch of 0.65 mm is giv...

Resolved! Minor error on reference manual RM 0410

Posted on March 22, 2018 at 17:49Hi in the reference manual for for STM32F76xxx and STM32F77xxx  which can be found here:http://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/96/8b/0d/ec/16/22/43/71/DM00224583/files/DM002...

LSI frequency range for STM32F303CC

Posted on February 13, 2018 at 13:16The current data sheet for the STM32F303CC (DocID023353 Rev13) shows on page 80 the characteristics of the LSI oscillator.Its frequency starts from min. 30kHz to typical 40 and max. 50 kHz (all at 3.3V in the max....