STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F303ZE Reference Manual clarification needed.

Posted on August 24, 2017 at 22:04HelloI'm about to start a project and the STM32F303ZE seems like a perfect part. I was reading through the Reference Manual and I found in the section 15.3.11 Channel selection (SQRx, JSQRx) that the ADC1 is connect...

m4l490n by Associate III
  • 178 Views
  • 2 replies
  • 0 kudos

STM32(F4) register programming

Posted on August 08, 2017 at 18:56Hi,I would like to programm my mcu (stm32f4) directly with the reference manual. Are there some examples from ST to see how it is done? I would need for the start examples of: I'C and GPIO.Hope you could help me,tha...

STM32L432KC: which reference manual should I use ?

Posted on May 19, 2017 at 08:30Hello everyone,Can somebody please explain me what are the differences between RM0393 (which is specific to STM32L4x2, but latest release is from May 2016) and RM0394 (which is specific to STM32L43xxx and so on and lat...

Kraal by Senior III
  • 178 Views
  • 2 replies
  • 0 kudos

STM32F1xx SCB::ICSR::VECTACTIVE field - R/W or RO?

Posted on May 04, 2017 at 16:08Hi there. According to PM0056 (4.4.3) VECTACTIVE field of ICSR register has read-write access. But in ARM DUI 0552A (4.3.3) this field marked as read-only. The latter looks more logical, because the rest of ICSR ignore...

STM32F746VGT6 Pinout

Posted on November 24, 2016 at 23:38I'm trying to build a custom PCB to control an graphic RGB 24 Bit TFT LCD.It seems I cannot find any were in the datasheet pins for LCD_R0 and LCD_B1 on an LQFP100 package.Can anyone help me, or explain why are th...

luchiann by Associate
  • 127 Views
  • 1 replies
  • 0 kudos

Registers datasheet

Posted on July 12, 2016 at 17:42Hi, I am currently using the STM8L152C6 MCU but I can not find the datasheet about registers.I looked at all datasheets present on this http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-...

0690X00000605bGQAQ.png 0690X00000605bLQAQ.png
thibaut by Associate
  • 195 Views
  • 2 replies
  • 0 kudos

BUG in STM32F030 reference manual.

Posted on July 01, 2016 at 14:56The register descriptions of the USART mention several times that the feature is optional and might not be implemented on my device (or my specific usart). I've seen such a table with other peripherals, but I can't fi...