STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405 CAN RX interrupt halts?

Hello, everyone.  I hope you're doing well.my work at this time: https://github.com/MarginallyClever/Daisy-Driver-2.0-firmware/commit/465ec3dbeb831ee2f49fd6a6648da8fd7377a56aMy code is written in Arduino 2.2.1 with https://github.com/stm32duino/Board...

CAN Wakeup

HelloI am trying to implement CAN Wakeup functionality. I have used MCP2562 Transceiver. I understand MCU will PU the stdby pin of Transceiver before going to sleep. By Pulling Up stdby pin, Transceiver will be in low power state and can still send s...

Nico3 by Associate III
  • 119 Views
  • 0 replies
  • 0 kudos

Resolved! CAN register not taking any data - STM32F4

Hey all,I’ve recently encountered an issue with setting up the CAN module on my STM32F4 and hope that someone is able to help me:After buying the SN65HVD230 CAN Board, I tried to set up the MCU so it can communicate with the CAN Bus. For that I solde...

SalomonD_0-1694689943730.png
SalomonD by Associate
  • 207 Views
  • 2 replies
  • 0 kudos

STEVAL-ESC001V1 CAN interface

I am looking for information regarding the CAN interface on the STEVAL-ESC001v1 board. In the features of the device it lists CAN as a feature but the documentation does not provide additional information on how exactly the CAN interface can be used ...

Resolved! CAN communication nucleo-f411re

Hello !I am currently trying communication using the CANBUS from a nucleo-f411re to an arduinoI used to work with an MCP2515 (using the CS, MOSI, MISO, SCK pins) and i now want to work with an MCP2551 using the RxCAN and TxCAN pins. My setup looks li...

lfresnay by Associate II
  • 360 Views
  • 5 replies
  • 0 kudos

CAN Messages not sending

Hi, I am using the following:cubeIDE 1.13.1/STM32F072C8U6/baud = 250K - I attached a picture of my clock diagram & param setup.Hi, I am using the following:cubeIDE 1.13.1/STM32F072C8U6/baud = 250K - I attached a picture of my clock diagram & param se...

DBles.1 by Associate II
  • 171 Views
  • 0 replies
  • 0 kudos