STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bluetooth module with high speed

Posted on September 06, 2017 at 09:11Hello,I'd like to create signal processing station based on STM F7 MCU and want to send input and processed data using bluetooth to other device. Could you recommend bluetooth module to do such thing? I know, the...

STM32F103 UART1 flow control + bluetooth BT121

Posted on August 01, 2017 at 11:56Hi all,I've a problem on STM32F103RET6 microcontroller using the UART1 flow control in combination with the Bluegiga BT121 bluetooth chip. I'm using a custom board with these simple hardware configuration:I'm using ...

0690X00000607k1QAA.png

SensorTile read the characteristic quaternions

Posted on March 03, 2017 at 09:59HelloMy company bought the STEVAL-STLKT01V1.I have to get the values of the quaternion's characteristic but it seems to be blocked.In fact with my computer i can : _ Connect in BLE to the sensorTile _ Get all service...

IDB05A1 - Help me decipher HCI event

Posted on February 13, 2017 at 12:56 I amsuccessfully able to communicate with my IDB05A1 from my nucleo-64 board. I make it discoverable and pair my phone to it. However immediately after pairing, the device disconnects from my phone. Befo...

HC-05 & HC-06 Bluetooth receiving wrong data usart

Posted on September 29, 2016 at 23:10 Hi, I got two STM32 board which I'm trying to send data through one and receive it on the other board through bluetooth. I have configured the HC-05 as master and it connects to the HC-6 successfully....

dragomir by Associate
  • 186 Views
  • 2 replies
  • 0 kudos

BlueMS source code

Posted on October 30, 2015 at 10:46Hi,I am working with bluemicrosystem1 application,for further expansion of my project BlueMS app source code is mandatory.In some of the sites it showing as it is available on Github. Anyone have this source code?P...