STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interface Bluetooth module(BL652) to stm32f7 series.

Hi All,Currently I am working on stm32F756 eval kit. I want to interface bluetooth in my project. As per requirement I have to use BL652 bluetooth module. As far I understand, nordiac semiconductor nrf5x SDK is required for BL652. I am new to bluetoo...

phenom by Associate II
  • 110 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-IDB05A1 with STM32F4-DISCOVERY

Posted on January 08, 2018 at 14:35Hi,I'm trying to port (use) X-NUCLEO-IDB05A1 board with STM32F4-DISCOVERY.I've begun developing this project by modifying SensorDemo for Nucleo-L053R8 board.I'm using Keil-MDK v5.25 (Lite). STM32F4 project is build...

About L2CAP protocol with STM32 + BlueNRG

Posted on June 14, 2018 at 10:12I'm new to BLE and I am confused with the L2CAP protocol. I've read the Bluetooth Core specification related to L2CAP and I understood that it provides in particular Segmentation and Retransmission capability ( which ...

Question on SBBTLE-RF module and the ST's API

Posted on May 31, 2018 at 10:46Hello,I'm using the SPBTLE-RF module (shield) with a nucleo (STM32L476RG). I use the sampleAppTht project given by ST.The SPBTLE-RF module is used as a server.I've have a few questions:   -the function aci_gap_set_disc...

NRST pin on STSPIN32F0A

Posted on December 07, 2017 at 10:55NRST � I/O Reset - Device reset input/internal reset output(active low). How can I connect this to a HC-05 bluetooth module?#stspin32f0a #bluetooth #nrst-pin #hc-05