STM32CubeMX (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Invalid SRAM6 Warning for U5A5ZJT6Q

Operating System: Windows 10STM32CubeMX version: 6.10.0STM32CubeU5 Firmware Package V1.4.0 / 20-October-2023When I attempt to validate my X-CUBE-AI model on target, I receive the following pop-up:Exploring STM32CubeMX.log shows the following warning:...

EdgyAI_0-1701470114151.png
EdgyAI by Associate II
  • 321 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U5A5 : GPMDA Linked List, what is Datasize

pNodeConfig.SrcAddress = &(ADC1->DR); pNodeConfig.DstAddress = (uint32_t) adc_values_1; pNodeConfig.DataSize = 4*64;In reference to the above based on an excellent tutorial (STM32U5 Workshop) which I use for nucleo STM32U5A5 https://www.youtube...

Riscy by Senior
  • 283 Views
  • 2 replies
  • 1 kudos

STM32U5 invalid SMPS warning during code generation

STM32CubeIDE 1.13.2 is showing a warning about SMPS for STM32U5 chips every time the code is generated (see attached).This is done even for chips which do not have the SMPS pinout, e.g. STM32U595VJT (non Q), which is completely invalid.But even when ...

Problem with IDE

Hello, I've got problem with STMCubeIDE. You can see my problem at photos I attached. Can anyone help me to solve this problem. I try to work on Lenovo Legion 5 with Ryzen 5 5600h and RTX3060. Second graphic card is integrated with Ryzen CPU. This pr...

STM32Cube Linked List generation issue

Hi all,I'm using STM32Cube IDE (version 1.13.1, build 17479_20230728_0839 ) to manage my company project based on a STM32U5 MCU.More specifically, I'm using linked list feature (for playing audio with SAI + DMA transfer) and I have noticed what appea...

fsorin by Associate II
  • 1132 Views
  • 9 replies
  • 2 kudos