MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB is returning zero as the sensor output

Posted on February 05, 2018 at 23:46After initializing an SPI 3-wire interface with a STM32L4 MCU on a custom board, the driver always returns zero as the pressure value whenever the get pressure method is called. Even the temperature sensor reading...

STM32 and VL53L0X

Posted on December 09, 2017 at 19:30Hey there,I'm working with my STM32L476 and the VL53L0X rangngs sensor.I'm using the Example from X-CUBE-53L0A1. I don't have the Nucleo board for the Sensor just a satellite board.  When using the example for ran...

Jonas L by Associate
  • 244 Views
  • 3 replies
  • 0 kudos

LSM303C issues

Posted on November 20, 2016 at 10:26Good morning,I'm developing an application on a STM32L4 discovery board which reads data from the lsm303c and logs those datas on the usb via an otg cable.The issue is that after few seconds the accelerometer stop...

How to download iNEMOEng_M1LI3 source code ?

Posted on April 01, 2016 at 15:09Either from http://www.st.com/web/en/catalog/tools/FM147/CL1818/SC1528 or http://www.st.com/web/catalog/tools/FM147/CL1818/SC1528/PF260129♯ it is impossible to download the source code to port on STM32L4 and support...

Noyb by Associate II
  • 192 Views
  • 0 replies
  • 0 kudos