MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I am using B-L475E-IOT01A board in that I am using Accelerometer sensor to read the vibrations that will be in time dominie , I want to convert into frequency dominie for that FFT is required. so, I want FP-CLD-WATSON1 package library required.

FP-CLD-WATSON1 package library file will support to plot FFT graph..can any one share link of that library file.. I could not found that.Thanks in Advance...

DNani.2 by Associate
  • 238 Views
  • 2 replies
  • 0 kudos

How to integrate LSM303AGR in STM32CubeIDE with STM32L4

Hey all! I'm doing a client project where I'm integrating an LSM303AGR on a custom board. I've included the XCUBE-MEMS package into STM32CubeIDE, and selected the LSM303AGR and set the I2C settings in the platform settings. This gives me LSM303AGR.C/...

Where are the .ioc files for STSW-STLKT01 sample programs?

According to the data brief STSW-STLKT01 Embedded software samples for SensorTile (DB2962) the sample projects are "Built on STM32Cube software technology, it includes all the low level drivers to manage the on-board devices and system-level interfac...

HCohe.1 by Associate III
  • 304 Views
  • 1 replies
  • 0 kudos

Resolved! Why do my I2C HAL commands to the LSM303AH not work?

When power is applied to the STM32L476, 3.3 v is also applied to the LSM303AH pins2             CS9             Vdd 10           Vdd IOThese commands work:MX_I2C3_Init();                      Goes to code created by CubeMX HAL_I2C_GetState(&hi2c3);  ...

JBonn by Associate III
  • 297 Views
  • 1 replies
  • 0 kudos

I'm working on a Sensortile.box for the first time. I'd like to create an app that records steps, activity type, and axis information (gyro) for three days straight. Would appreciate any insight for a newbie here. Questions below:

I'm working on a Sensortile.box for the first time. I'd like to create an app that records steps, activity type, and axis information for three days straight. Would appreciate any insight for a newbie here. Questions below:How would you program an ap...

Resolved! X-Nucleo-IKS01A2 and Nucleo-L496ZG

Hello,I would like to know about the integration between Nucleo-L496GZ with X-Nucleo-IKS01A2 sensor board.Is there really no example that facilitates the integration of these boards?There really is no example using the Nucleo-L496ZG integrated with s...

GThab.1 by Associate II
  • 225 Views
  • 1 replies
  • 0 kudos

Resolved! Free fall detection in LSM6DSO not working.

Hello everyone!I got LSM6DSO on my custom board with stm32l4 MCU, I only use I2C interface (that i don't use interrupt). I'm using LSM6DSO free fall example code in STMems standard C drivers, I can get the id of LSM6DSO so i think the I2C interface ...

DDuc .1 by Associate II
  • 593 Views
  • 9 replies
  • 0 kudos