MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX X-NUCLEO-IKS01A2 X-CUBE-MEMS1

I Refered to Page 25 ,7.1 of the Document and Used of MEMS Library without sample applications for XNUCLEO-IKS01A2 with NUCLEO-L4R5ZI. in the platform setting there is no BSP_BUS_DRIVER ,i2c。another problem is that BSP_USART has no solution. Who kno...

0690X000008wDNFQA2.png 0690X000008wDNKQA2.png
Fgg by Associate II
  • 162 Views
  • 0 replies
  • 0 kudos

CubeMX + NUCLEO-L053R8 + X-CUBE-MEMS1 can't be built

Using CubeMX v5.0 and FW_L0_v1.11.0 I'm generating new project from scratch.Project has initialized (using HAL) UART2, I2C1 (on alternate pins PB8, PB9), GPIOs, EXTIs and clock. UART2, I2C1 and EXTI interrupts are enabled and IRQ handlers generated b...

Connecting the API with STM32 platform in CubeMX

Posted on February 13, 2017 at 16:04HiIm having the device VL53L0X which I want to communicate with trough the I2C protocol to my STM32F401RE micro controller.Im using CubeMX from STM to setting up the pins which works fine, but I don't know how I '...

STM32F429 Audio USB with CubeMX

Posted on May 06, 2015 at 13:02Hello, I have a quick question, and I cannot find answer anywhere on the web (including Reference Manual for MCU). I'm preparing for a new project, picking master unit, where one of most important feature is USB audio ...

axel2 by Associate II
  • 627 Views
  • 4 replies
  • 0 kudos