STM32 MCUs Wireless

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[BLE RSSI] Reading RSSI value uint8_t

Hello, I am working with STM32WBA52CG as a central and I want to read the RSSI from the incoming advertising packets. The RSSI value should be a negative value in dBm, however it is defined as uint8_t in the AdvertisingReport_t structure. Can someone...

Screenshot from 2024-02-12 10-41-02.png
Portilha by Associate II
  • 718 Views
  • 17 replies
  • 2 kudos

Problem with DMA from FLASH on STM32WBA52

Hi all, I am experiencing a problem with the DMA of the STM32WBA52 (on the NUCLEO-WBA52CG board) when using it to transfer data from FLASH to USART1 TX : part of the transmitted data is modified, i.e. not the data that is found in FLASH)The problem o...

jeroen by Associate III
  • 556 Views
  • 2 replies
  • 0 kudos

STM32WBA52 Serial Port Emulation

Hello,I am developing a Bluetooth application which can communicate with Android phone emulating Serial Connection. On previous device we used our own Bluetooth Classic module with SPP (Serial Port Profile) using RFCOMM (Serial Port Emulation) and we...

DLich.3 by Associate II
  • 466 Views
  • 3 replies
  • 1 kudos

NUCLEO-WBA52CG Corrupted BLE Hardware on PC

Hello, I am using 2 NUCLEO-WBA52CG dev boards with project STM32Cube_FW_WBA_V1.1.1\Projects\NUCLEO-WBA52CG\Applications\BLE\BLE_p2pServer. I am using IAR 9.40.1 My pc wireless is Intel® Wi-Fi 6 AX200, pc is running win10 pro (latest) While getting th...

Working Unit - Add a device.png

Resolved! STM32CubeMonitor-RF for testing BLUENRG-M2SP

Hi,I want to use the BLUENRG-M2SP for an application and I want to test this BLE module before designing a HW. For this, I have a NUCLEO F411RE and a NUCLEO BNRG2A1.I wonder if it's possible to use STM32CubeMonitor-RF as a serial terminal in order to...

dsm85 by Associate
  • 248 Views
  • 1 replies
  • 0 kudos