STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Race condition in UART_RxISR_8BIT (HAL)

The error occurred while reading a UART interface (heavy load @ 115200 baud) byte by byte (with HAL_UART_Receive_IT(&huart1, &com_uartRxSignBuffer, 1) ). MCU: STM32F302VB ST firmware version : STM32Cube_FW_F3_V1.11.2Before the RXNE interrupt is disab...

Blacbird by Associate II
  • 710 Views
  • 6 replies
  • 1 kudos

USB HID Device response with a STALL

Hello everyone,I have trouble while implementing USB HID on a STM32F373.I use the "custom Human Interface device class" and implemented all like in the video from ST Link. I also tested my device with the HID Terminal from the video (the Programm jus...

0693W00000HneolQAB.png
DSchu.6 by Associate
  • 209 Views
  • 0 replies
  • 0 kudos

Resolved! Nucleo-F303RE USB HID Not working

I'm prototyping a project, and im struggling to get USB HID working on the Nucleo F303RE board. I've connected an external micro-usb breakout board to the nucleo via the PA12 & PA11 pins as configured in the CubeIDE. However running the most basic us...