STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to setup CMSIS DSP on a ARM Cortex M33

Hello Everyone,I currently trying to implement a FFT by using the optimized functions from CMSIS library on a L5 MCU. The fact is that the M33 family seems not to be supported then I was wondering whether there's some kind of workaround in order to m...

bedo98 by Associate
  • 1466 Views
  • 3 replies
  • 0 kudos

Resolved! CMSIS DSP Library performance

I'm using the STM32F769DI and the SMT32cCube for a project which will be using the CMSIS DSP libraries in a computationally demanding application.My C code is set for fast optimisation. __FPU_USED and FPU_PRESENT are set. ARM_MATH_CM7 is defined. I c...

IWhit.2 by Associate II
  • 1329 Views
  • 3 replies
  • 0 kudos

Resolved! How to use CMSIS 5.8.0 in the cubeIDE

Hi,I use the stm32f446re with the cubeIDE and would like to use FFT's with 16 bit float (arm_rfft_fast_f16) like in the CMSIS DSP 5.8.0.The older CMSIS library works fine with the other data types but i cant get the new (DSP 1.9.0) to work. I tried d...

MH081 by Associate
  • 466 Views
  • 2 replies
  • 0 kudos