2026-01-20 10:00 AM
I hope this short guide will help some of you. Feel free to reach out if you have any question.
Solved! Go to Solution.
2026-02-26 7:03 AM
Hello @cp5900 @,
Thanks for sharing this case and the solution you found.
To make this post more visible and easier to find by others who may face the same issue, I mark my reply as the solution.
@cp5900 wrote:
Context : I want to write a FSBL load and run application on a custom minimal PCB based on STM32N6-DK design. The board uses SMPS power supply and not the default power supply of the STM32N6-DK. I follow this original tutorial as a main example.Problem faced: CubeProgrammer SigningTool version compatibility and header size1) Write a custom external bootloader to write and read external flash memory
- Modify the power supply parameter (System Core --> RCC --> SupplySource) in CubeMX to `PWR_SMPS_SUPPLY`
- Generate ExtMemLoader template from CubeMX
- Build ExtMemLoader to generate .stldr file
- make sure the post build script can be executed
- manually copy the .stldr file generated in `/STM32CubeProgrammer.app/Contents/Resources/bin/ExternalLoader/` if necessary
2) Modify SigningTool header generation command in FSBL post-build
- Build FSBL & Application following the original tutorial
- Check heading size, it might be different from the 0x400 that is defined in CubeMX (caused by uninstalling then reinstalling CubeProgrammer thus SigningTool)
- look for this message *[Header v2.3] Do not align the payload to the 0x400 offset, No padding bytes at the beginning of the payload*
- Vector Table cannot be located at 0x240 for hardware alignment constraint, therefore it needs to be at 0x400 (following the header)
- Add `--align` at the end of the SigningTool command to add padding bytes and get a 0x400 header (`STM32_SigningTool_CLI -bin FSBL.bin ... --align`)
- Then rebuild and make sure header size is 0x400
3) Program flash and debug
- Select the custom .stldr as External loaders in CubeProgrammer
- Write trusted.bin files for both FSBL and Application following the original tutorial
- To use the Debugger in CubeIDE you also need to add the custom .stldr file previously generated in Debug Configurations --> C/C++ Application --> Debugger --> External loaders). Follow the instructions from this tutorial
I hope this short guide will help some of you. Feel free to reach out if you have any question.
Regards,
Maxime
2026-02-03 8:15 AM
Hi @cp5900,
Thank you very much for sharing, I believe this will be useful for future readers!
Have a good day,
Julian
2026-02-26 7:03 AM
Hello @cp5900 @,
Thanks for sharing this case and the solution you found.
To make this post more visible and easier to find by others who may face the same issue, I mark my reply as the solution.
@cp5900 wrote:
Context : I want to write a FSBL load and run application on a custom minimal PCB based on STM32N6-DK design. The board uses SMPS power supply and not the default power supply of the STM32N6-DK. I follow this original tutorial as a main example.Problem faced: CubeProgrammer SigningTool version compatibility and header size1) Write a custom external bootloader to write and read external flash memory
- Modify the power supply parameter (System Core --> RCC --> SupplySource) in CubeMX to `PWR_SMPS_SUPPLY`
- Generate ExtMemLoader template from CubeMX
- Build ExtMemLoader to generate .stldr file
- make sure the post build script can be executed
- manually copy the .stldr file generated in `/STM32CubeProgrammer.app/Contents/Resources/bin/ExternalLoader/` if necessary
2) Modify SigningTool header generation command in FSBL post-build
- Build FSBL & Application following the original tutorial
- Check heading size, it might be different from the 0x400 that is defined in CubeMX (caused by uninstalling then reinstalling CubeProgrammer thus SigningTool)
- look for this message *[Header v2.3] Do not align the payload to the 0x400 offset, No padding bytes at the beginning of the payload*
- Vector Table cannot be located at 0x240 for hardware alignment constraint, therefore it needs to be at 0x400 (following the header)
- Add `--align` at the end of the SigningTool command to add padding bytes and get a 0x400 header (`STM32_SigningTool_CLI -bin FSBL.bin ... --align`)
- Then rebuild and make sure header size is 0x400
3) Program flash and debug
- Select the custom .stldr as External loaders in CubeProgrammer
- Write trusted.bin files for both FSBL and Application following the original tutorial
- To use the Debugger in CubeIDE you also need to add the custom .stldr file previously generated in Debug Configurations --> C/C++ Application --> Debugger --> External loaders). Follow the instructions from this tutorial
I hope this short guide will help some of you. Feel free to reach out if you have any question.
Regards,
Maxime