2025-12-17 5:40 AM
Hi
After the latest update, I can't download C Code from Edge Ai Developer Cloud, there are no boards in the list.
fv
Solved! Go to Solution.
2026-01-09 5:24 AM
This should be fixed.
2025-12-17 8:16 AM - edited 2025-12-19 1:49 AM
Hi @francovaro,
This is indeed the case. it seems to be a bug for now.
So how to work in the meantime? it depends on your target:
Non NPU target:
We advise that until March, for "normal" stm32, you use the version 2.2 of the core (so X cube AI 10.2 and you should also be able to use it in the dev cloud). This is because the new 3.0 version is mainly a NPU improvement.
For NPU target (your case):
CubeMX do not really support the N6 correctly, so everything is available directly in the ST Edge AI Core install folder. Which means that you can use the 3.0
The validation application is in C:\ST\STEdgeAI\3.0\Projects\STM32N6570-DK\Applications\NPU_Validation
Here is a guide on how to use it, for more details please visit: https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_getting_started.html
Then edit the config.json file, here is mine for reference:
You need STM32CubeIDE and most paths can be found by going to the pluging folder of the local install of STM32CubeIDE, searching for each element and copying the path.
With the configuration done, you should not have an error. If you get an error for the make path, add it to the configuration file. This is what you should get:
Finally, run the following validate command:
stedgeai validate --model ./models/model.onnx --target stm32n6 --mode target -d serial:921600
Note: if you unplug the N6, you will need to reflash the validation firmware with the n6_loader.py before running the validate command.
by default, it uses random data as input. It would be better if tested on a real input dataset using the option: -–vi dataset.npz
It can take quite a while, but you should get something like this:
Have a good day,
Julian
2026-01-09 5:24 AM
This should be fixed.
2026-01-14 3:42 AM
Yes it's fixed!
thank you