Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeAI-Keras Sequential model with multiple inputs gives INTERNAL ERROR: unpack_from requires a buffer of at least 4 bytes

I've followed this tinyML for stm32 from Digikey "TinyML: Getting Started with STM32 X-CUBE-AI | Digi-Key Electronics" reference,and got no Errors in STM32CubeMX when I clicked "Analyze" button after I've uploaded the tfLitemodel.Later I've tried thi...

Unable to use [validate on target] with cubeAI

Hi all,​I tried to porting AI model which I made with cubeAI but it seems like not work.​I succeded [validation on target] once but I don't know how I could do this.​​​​When I run [validation on target], it respone that it cannot find NetworkRuntime7...

0693W00000Su3RYQAZ.png 0693W00000Su3SRQAZ.png 0693W00000Su3o8QAB.png 0693W00000Su3pfQAB.jpg
MYu.3 by Associate
  • 685 Views
  • 0 replies
  • 0 kudos

Resolved! Can STM32WL be used with STM32Cube.AI ?

Noob question - can I use AI with the STM32WL SoC ?I want to train a model and then use STM32Cube.AI to put it on STM32WLE5CC. This is so I can use AI on the end device and transmit data using LoRa all using the one chip.Is this possible ?Many thanks...

Running an AI model in Low-Power?

Hi,I'm working on an application on a STM32WB55 which is sampling sensor data with 52Hz and feed it into a Keras model. Both the raw sampling sensor data as the output of the model will be saved to external flash memory (every 64 samples). A 52Hz int...

F F by Associate II
  • 1161 Views
  • 1 replies
  • 0 kudos

How to use CLI to find SRAM/Flash usage of TFlite model in X-Cube-AI

I realize you can use the stm32ai tool to find the SRAM/Flash usage of the model. However, this does not include the "Library" size. This "Library" size is only calculated when you click analyze in Cube IDE. See above image. How do I calculate "Libra...

0693W00000QNpz0QAD.png
TZieg.1 by Associate
  • 590 Views
  • 0 replies
  • 1 kudos

SensorTile - SD card is missing

Hello.I evaluate the SensorTile Kit with the following combinations.Core system STLCS01V1Cradle expansion STLCX01V1​When I connect to the Android app "ST BLE Sensor" and select "AI Data Log" to collect learning data, I get an error saying "SD Card is...

gocchan by Associate III
  • 712 Views
  • 0 replies
  • 0 kudos