Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST is Looking for Data Scientists – Join a paid usability session

Hello Community,   ST is Looking for Data Scientists – Join a paid usability session   Are you a data scientist or ML engineer with experience deploying neural networks on edge or embedded devices? The ST team is organizing 45-minute remote usability...

Understanding Object Detection AI Output

Hello everyone!At the moment I am developing an AI system for the STM32H7A3 using STM32 Model Zoo und Cube AI. For testing purposes I trained the SSD Mobilenet V1 model for 192x192 picture resolution and implemented it in a firmware app for testing i...

haraldN by Associate
  • 1041 Views
  • 0 replies
  • 1 kudos

Resolved! Detection of unwanted noise in cars (Sensortile.box)

I'm trying to do a program like a baby crying and i'm looking for the code of babycrying program. I need to do a program that detects unwanted noises in cars, so i think that maybe is similar than the babycrying app.I thought it was possible using th...

SAbba.1 by Associate III
  • 2385 Views
  • 5 replies
  • 1 kudos

Integration of AI in old CubeMX project

Hello everybody,I started to use the AI Cube MX extension and developed an application on the NUCLEO-F746ZG Board. It all worked very well.Now I am trying to integrate this small application into a bigger, existing project.There seems to be a problem...

Neural Network / Classification

Good morning, I am working on this Firmware https://github.com/stm32-hotspot/STM32WB-BLE-AI-MotionSense.I created the Neural Network but I don't see the Classification on The Monitor.Can you help me to solve the problem ?Thank you.Best regardsLuigi B...

Resolved! How to use external Flash with STM32Cube.AI?

Hi,I have managed to program the STM32F746G-DISCO with a simple neural network but when I try to do it using the external Flash by using the option in advanced settings (External NOR Flash) it doesn't work. Any idea why? Is there anything else I need...

DPast.2 by Associate
  • 2222 Views
  • 2 replies
  • 0 kudos

Keras 2.12.0 support

I want to know when will stm cube ai support keras 2.12.0 because for now it only support up till 2.11.0. I can't seem to downgrade my keras version as it require to downgrade more dependencies.Furthermore I converted my lstm keras (h5) model to tfli...

UAtif.1 by Associate II
  • 2205 Views
  • 5 replies
  • 0 kudos

Error analyzing a model with custom layers

I am using the XCUBE-AI software to deploy an SNN (Spiking Neural Network) on my STM32H747I-DISCO board. The SNN is in the form of a .h5 file, and was converted from a CNN using the snn toolbox. The SNN ofcourse, has a lot of custom layers. I want to...

running on target validation on STM32Cube IDE and XCube AI

I have a saved tflite model , which I want to deploy on my STM32H747I-DISCO board. For now, I just want to run validation on target using one custom input. I have the input as a numpy array (saved as a .npy file, it's a 4D array). Can someone please ...

SMehr.2 by Associate
  • 1062 Views
  • 0 replies
  • 0 kudos