Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am starting an APP with AI

Hello good afternoon, I am starting to make an application with the sensortile.box very similar to "baby crying". I would like to ask if you have any information that can support me in this process, for example to activate the use of the AI folders i...

SAbba.1 by Associate III
  • 904 Views
  • 1 replies
  • 0 kudos

About Yolov5 being unable to be deployed on CubeAI when transitioning to Onnx

我真的不知道为什么..将出现此问题。将 YOLOv5 转换为 ONNX 后,我无法在其上部署它,因为我的显卡是 1660ti 并将半精度转换为单精度。如果我使用半精度,它可能不支持 16 位半精度(所以要减小我的权重文件的大小并不容易),但如果我切换到单精度,则意味着列表溢出,并且没有指示溢出发生的位置。我真的很相信,事实上,我还没有看到一些 Yolov5 部署在 cubeAI 上......一些大人物知道为什么在这里

微信图片_20230714085808.png 微信图片_20230714085752.png

Resolved! Anomaly detection argumente,

Hello every Body, i am investigating the use of ISM330IS with nanoEdgeAI to detect Anomaly situations. Lets take a motor for air conditioning as an example, If the motro  has protection against high current, and a tachometer, What are the benefits of...

How can I use QKeras models with X-Cube-AI?

Hi, I am trying to use a QKeras model with mixed precision on STM32H747I-DISCO board. I run ‘Analyze’ my QKeras model using stmai 8.1.0, but encountered the following error. I tried an old version of QKeras, but got a different error. I would appreci...

Unable to include header file

Hello! Im using STM32Cube IDE version 1.12.1.Im having isssue with including the header file "ai_platform.h " and "ai_datatypes_defines.h".I have installed X-cube-AI extensions  and all other required extension of Artificial Intelligence.I am getting...

Unicleo-GUI

Good Morning , I am working on the following board:  https://www.st.com/en/evaluation-tools/stm32wb5mm-dk.htmlI need to activate Unicleo-GUI and MLC core on the board.  Do you know how to get it ?Thank you very much. Best regardsLuigi Bibbo'PS: my em...

I can't compile the AI project on the STM32H743 chip

How to deal with fatal error: ai_platform.h: No such file or directory? I can't find this file anywhere in the project.I tried using different versions of CubeIDE and X-CUBE-AI, added include paths in project properties. I checked on F7 and H7. I hav...

_legacyfs_online_stmicro_images_0693W00000biWOuQAM.png _legacyfs_online_stmicro_images_0693W00000biWNzQAM.png
RPuch.1 by Associate II
  • 2487 Views
  • 3 replies
  • 1 kudos