Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Trigger delay in Machine Learning Core feature detection

Hello,I’ve been trying to figure out how fast the machine learning core on the LSM6DSOX can generate an output once the condition for the change has occurred. I am working on a design where feature detection is needed in less than 50ms. I am using th...

EC.2 by Associate II
  • 3170 Views
  • 5 replies
  • 0 kudos

cube AI generated code error

When trying to use ai_network_ai_params, I get this error during the build process(my model name is sine_model). How do you fix this? Build error message:../Middlewares/ST/AI/Inc/ai_platform.h:323:4: error: 'union <anonymous>' has no member named 'fo...

LKan.1 by Associate II
  • 3753 Views
  • 7 replies
  • 2 kudos

How to run "validate on target" in with cube-x-ai

I am using a Nucleo-F676ZI and trying to run a dnn on the mcu. I can run the NN using the "application template" but I want to use the "validate on target" in order to obtain runtime without developing the data transfer from the host system to the mc...

0693W00000FBuMeQAL.png 0693W00000FBuK0QAL.png 0693W00000FBuOaQAL.png 0693W00000FBuPsQAL.png
MKlem.2 by Associate II
  • 2879 Views
  • 4 replies
  • 2 kudos

Deploy NN models on STM32L4R5ZI-P

I'm new to use STM32 boards. I have encountered problems when I try to deploy a pre-trained NN model on STM32L4R5ZI-P. When I have converted my NN model by using STM32cubeAI embedded in STM32cubeMX. It gives me a project folder. What should I use to ...

CShen.1 by Associate
  • 5741 Views
  • 1 replies
  • 1 kudos

Hey guys, could you help me out and provide some guidance in speech recognition small project. I using STM32L476 and i want to create speech recognition on this thing. I've got an model created in Python for 2-3 simple words.

Hey guys,could you help me out and provide some guidance in speech recognition small project.I using STM32L476 and i want to create speech recognition on this thing. I've got an model created in Python for 2-3 simple words and how do i go from here, ...

FP-AI-VISION1 - Object Detection starting point

Hi ST,I would like to use the project 'People counting' in FP-AI-VISION1's function pack on my ST32H747-DISCO board + B-CAMS-OMV. The idea is to replace the model with a specific object instead of a person.Now there is only a binary file available to...

eeeeee by Associate III
  • 1022 Views
  • 1 replies
  • 1 kudos

X-Cube-AI Calculation of Memory Requirements

I would like to compare a lot of CNN models in terms of RAM usage.If I analyze a single model the important result I am interested in is the ram (total) usage. As that practically defines, if the model fits into the RAM. weights (ro)         : 1,544 ...

0693W00000FDSY2QAP.png
MKlem.2 by Associate II
  • 910 Views
  • 0 replies
  • 0 kudos