Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST is Looking for Data Scientists – Join a paid usability session

Hello Community,   ST is Looking for Data Scientists – Join a paid usability session   Are you a data scientist or ML engineer with experience deploying neural networks on edge or embedded devices? The ST team is organizing 45-minute remote usability...

Resolved! Use External Flash (QSPI) for CubeAI weights

Hi all,I would like to ask if there is a suggested procedure to move the network weights, the one generated inside network_data.h, to external memory-mapped QSPI FLASH. I've already moved both input/output data and activation to external SRAM, but I'...

Raggio by Associate III
  • 1704 Views
  • 3 replies
  • 0 kudos

STM32F serial deep/machine learning development board

I am looking for a development board that can run a deep learning model with a CSI interfaced CMOS camera.I think if chips can support DCMI(digital camera interface), it means it is available for CSI interfaced CMOS cameras. I hope my idea is right. ...

FWu.3 by Associate III
  • 599 Views
  • 0 replies
  • 0 kudos

no source available for "ai_platform_inputs_get()" X-cube.AI version 7.1.0 I attach a basic code snippet which might be helpful in recreating the problem

/* USER CODE BEGIN PV */ static ai_buffer *ai_input; static ai_buffer *ai_output; /* USER CODE END PV */   int main(void){ ... // Chunk of memory used to hold the intermediate values for neural network AI_ALIGNED(32) ai_u32 activations[AI_NETWORK_D...

Resolved! Explanation of FFT display in NanoEdge AI Studio

I am using your NanoEdge AI Studio Software for classification and I am looking at the FFTs displayed in the signals segment after collecting data.How, specifically are these FFTs generated from the raw data ? Also, what the units on the axis are as ...