Skip to main content
robertabel9
Associate
November 18, 2016
Question

Information on patch.xml workflow

Posted on November 18, 2016 at 17:38

I'm currently using SPC5Studio 4.2.1 (4.2.1.201607051420) and use it to develop on an SPC560B-DIS evaluation board. I noticed that edits I make to component files in the lib sub-directory are handily stored in regular diff format in patch.xml.

However, I would also like to edit files in e.g. the cfg sub-directory, so I manually created the following entry inside the patch.xml file:

<?
xml
version
=
''1.0''
encoding
=
''UTF-8''
?>
<
SPC5-Patch
version
=
''1.0.0''
>
<!--It is your patch repository, do not break your XML File.-->
<
files
>
<
file
componentId
=
''org.chibios.spc5.components.spc5hal''
version
=
''1.0.0.201607011046''
path
=
''component/cfg/halconf.h''
user
=
''false''
>
<
diff
>
<![CDATA[--- components/portable_spc5_hal_component/cfg/halconf.h
+++ components/portable_spc5_hal_component/cfg/halconf.h
@@ -79,7 +79,7 @@
* @brief Enables the I2C subsystem.
*/
#if !defined(HAL_USE_I2C) || defined(__DOXYGEN__)
-#define HAL_USE_I2C FALSE
+#define HAL_USE_I2C TRUE
#endif
/**]]>
</
diff
>
</
file
>
</
files
>
</
SPC5-Patch
>

However, these manually introduced patches aren't being applied once I recreate the component tree. Is there some setting/trick/... to enable this? Is my syntax wrong? Or is it plain not possible to patch files outside of the lib sub-directories at the moment? #spc5studio-patch
    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    November 21, 2016
    Posted on November 21, 2016 at 09:57

    Hello robert ,

    You can not patch a configuration file (cfg directory).

    cfg file is a file generated from the GUI.

    I2C driver does not exist on B Discovery (HAL & RLA)

    HAL Side : i2c_lld.c should be created

    RLA Side : i2c_lld.c should be created

    we have a change request to create I2C for B Discovery

    (i am writing a private email for you)

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    robertabel9
    Associate
    November 22, 2016
    Posted on November 22, 2016 at 14:31

    Hi Erwan,

    It's unfortunate that the cfg files cannot be patched. The reason I'm asking is that I implemented my own i2c lld interrupt-driven driver but use the ChibiOS hal to be compatible. So far I haven't received your private e-mail.

    Regards,

    Robert
    Erwan YVIN
    ST Technical Moderator
    January 18, 2017
    Posted on January 18, 2017 at 16:49

    Hello Robert ,

    You should check the post

    https://community.st.com/0D50X00009XkYQQSA3

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.