Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Where can I find the example project for JTAG over CAN?

I'm implementing JTAG over CAN as described in AN4345, "Debug over CAN". https://www.st.com/resource/en/application_note/dm00094335.pdfIn sections 5 and 6, mention is made of an example Greenhills project with the code described in the app note. Desp...

ehntoo by Associate
  • 963 Views
  • 0 replies
  • 0 kudos

Resolved! Not able to send the data without delay in UART interfacing. I am using 3 UART channel at a time. I want to know how can I remove the delay .

I am working with 560B54L5 discovery board. I am using runtime IO component with uart test application. I am able to send data at one channel at a time(one channel).my issues arehow to receive the data using interrupt in case of runtime IO?How can I ...

rpoon by Associate II
  • 1856 Views
  • 1 replies
  • 0 kudos

Resolved! Creation of a timer for continuous execution

I used the stm application fot configuaring the Timer.1.first picture shows the timer is working for just 4 seconds but i want it to run continously i used the stm_lld_enable inside the for loop and it is not working i dont know why.

RRama.8 by Associate II
  • 1852 Views
  • 2 replies
  • 0 kudos

Resolved! How to config with CAN bus filter in SPCstudio?

Hi all, I'm using SPC570S0DISP DEMO Board(SPC570S50E1) to lean how to config CAN's filter.And the attachment is my config and source code. In my config,i just want CAN ID 0x112 to interrupt fifo callback function.And then i get the data in call...

LJere by Associate
  • 1781 Views
  • 2 replies
  • 0 kudos

Resolved! Confused between set address for bootloader and 32-bit store address from UART/CAN flash while flashing

Hi,This is for SPC560Bxx. I need clarification on set address for bootloader and the 32-bit address that shall be mentioned on UART/CAN frame. There is one column in firmware updater component, where we are supported to choose it the set address, he...