STM32CubeMX 6.16.1 ignores .ioc settings for the "Generated Function Calls" table?
Hello,
I'm using the latest STM32CubeMX 6.16.1 (Linux version), and working on a project cloned from the one provided for STM32MP257F-DK.
In the Project Manager -> Advanced Settings, there is the "Generated Function Calls" table.
If I set checkboxes here, e.g. in the "Do Not Generate Function Calls" column, the generated code reflects the new settings. However, when I reload the project (via "close/open" or just restarting CubeMX), all checkboxes are in their default positions (disabled for all functions in "Do Not Generate Function Calls").
The same thing is with the first "Generate Code" column, and re-ordering the calls doesn't save as well.
Is there a workaround?
A question to STMicro engineers: enabling OpenAMP middleware for STM32MP2 boards fails to build in CubeIDE. Looks like it is a known issue https://community.st.com/t5/stm32-mpus-software-development/stm32mp257f-dk-openamp-no-such-file-or-directory/td-p/786509, is there a plan to fix it in the next release of CubeMX?
Thanks!
Regards,
Sergei