Skip to main content
mahmoud boroumand
Associate III
July 24, 2017
Question

ws2812 with multiple output

  • July 24, 2017
  • 2 replies
  • 703 views
Posted on July 24, 2017 at 13:38

Hello

i use stm32f103c8 and use this library 

https://github.com/g4lvanix/0xWS2812

  .it work without any problem in all pin(16 pin) of gpio.but it work on only one of the port (gpioa-gpiob) and i can olny use one of the port and 16 out put but i need 32 output.how can use two port at the same time?
    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    July 24, 2017
    Posted on July 24, 2017 at 13:49

    You can't. Use a second timer with suitable DMA channels.

    JW

    Tesla DeLorean
    Guru
    July 24, 2017
    Posted on July 24, 2017 at 16:13

    Asked and Answered

    https://community.st.com/0D50X00009XkXm1SAF

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..