Skip to main content
Sankalp Agarwal
Visitor II
July 3, 2018
Question

Wrong register bit assignment for ADC voltage regulator (ADVREGEN) for STM32F303VC

  • July 3, 2018
  • 1 reply
  • 678 views
Posted on July 03, 2018 at 13:10

In the System Viewer file -> ADC -> ADC1,ADVREGEN is assigned with

[Bit 28]

But as per the below link of reference manual RM0316, it should be

[Bit 29:28]

http://www.st.com/content/ccc/resource/technical/document/reference_manual/4a/19/6e/18/9d/92/43/32/DM00043574.pdf/files/DM00043574.pdf/jcr:content/translations/en.DM00043574.pdf

Thus we request you to provide updated SVD file for this device.

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    July 4, 2018
    Posted on July 04, 2018 at 12:26

    Hello 

    agarwalsankalp1989

     ,

    Thank you for bringing this issue to our attention.

    This is raised internllay for fix.

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks