Question
Why doesn't gdb reach a breakpoint in main?
Posted on December 17, 2014 at 17:43
Hello,
I'm trying to debug a simple test program (http://developer.mbed.org/teams/ST/code/Nucleo_blink_led/
) on my Nucleo board. I've successfully compiled it using GCC-ARM (arm-none-eabi-gcc), flashed my device over USB, and saw the light blink on and off. The trouble arises, however, when I try to actually step through my program. And yes, I made sure to enable debugging with the ''-g'' compile flag. Here's my terminal output. I start the gdb server daemon using OpenOCD...matt@ubuntu:~/Nucleo_blink_led$ openocd -f board/st_nucleo_f401re.cfg
Open On-Chip Debugger 0.8.0 (2014-05-10-23:20) Licensed under GNU GPL v2 For bug reports, read http://openocd.sourceforge.net/doc/doxygen/bugs.html srst_only separate srst_nogate srst_open_drain connect_deassert_srst Info : This adapter doesn't support configurable speed Info : STLINK v2 JTAG v19 API v2 SWIM v3 VID 0x0483 PID 0x374B Info : using stlink api v2 Info : Target voltage: 3.257255 Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints ...execute gdb in another window... matt@ubuntu:~/Nucleo_blink_led$ arm-none-eabi-gdb Nucleo_blink_led.elf GNU gdb (7.8-0ubuntu1+6) 7.8 Copyright (C) 2014 Free Software Foundation, Inc. ... Reading symbols from Nucleo_blink_led.elf...done. (gdb) ...enter a few commands...(gdb)
tar ext :3333
Remote debugging using :3333 gpio_write (obj=0x20000268 <myled>, value=1) at ./mbed/TARGET_NUCLEO_F401RE/TARGET_STM/TARGET_NUCLEO_F401RE/gpio_object.h:55 55 *obj->reg_set = obj->mask; (gdb) b main Breakpoint 1 at 0x80002a2: file main.cpp, line 7. (gdb) r The program being debugged has been started already. Start it from the beginning? (y or n) y Starting program: /home/matt/Downloads/Nucleo_blink_led/Nucleo_blink_led.elf Note: automatically using hardware breakpoints for read-only addresses. ...and get this output from OpenOCD.Info : accepting 'gdb' connection from 3333
Info : device id = 0x10006433 Info : flash size = 512kbytes target state: halted target halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x080004a4 msp: 0x20018000 Would somebody please tell me how to make sure that my program actually gets to main before halting, so I can step through it like I had originally meant to? Thanks in advance. #openocd #debug #arm-none-eabi-gdb