Skip to main content
VPras
Associate III
November 4, 2019
Question

what is the source of clock for CANBUS

  • November 4, 2019
  • 1 reply
  • 1069 views

Hi,

what is the clock source for CANBUS in STM32F767?

I have referred the manual ,but still i cannot get the clear answer from it.

the main reason to know the clock source is to calculate the bit timing .

Thanks

Vimal

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
November 4, 2019

Usually the APB to which it is attached.​

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
VPras
VPrasAuthor
Associate III
November 4, 2019

Hi,

my application is to create USB and CANBUS together.

1.when i use 16MHz crystal oscillator, i kept all PLL settings for max clock ,then USB is not working.

2. when i use 25MHz crystal oscillator ,CAN is not working.

what could be issue??

Thanks,

Vimal