Skip to main content
taha_najmee
Associate II
February 25, 2013
Question

USB CDC Driver

  • February 25, 2013
  • 1 reply
  • 606 views
Posted on February 25, 2013 at 23:52

Hello,

Can someone inform me whether I can use (or do I need) USB CDC Driver on Windows CE. I am planning to connect STM32F4 Discovery to Cuwin Touch Screen panel which is operated on Windows CE.

I checked the 'readme' file which comes with the driver and it says it is only compatible with Windows 98 SE, 2000, XP, Vista, 7.

Thanks for the help
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    February 25, 2013
    Posted on February 26, 2013 at 00:33

    WinCE is NOT compatible with drivers from those other Microsoft operating systems, and in many cased doesn't even use an x86 CPU.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..