Usage of HAL_SPI_Transmit
Hi,
normally i use HAL_SPI_Transmit
HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(...)
HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_SET);
Is it possible to use it like following;
HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(...buffer1..)
HAL_SPI_Transmit(..buffer2..)
HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_SET);
Thank you
Note: The reason I need to use it like that is that, I need to call it in a function, which takes buffer1 and buffer2 as parameter; function(.., uint8* buffer1, uint8 buffer2, )