Skip to main content
danesh
Associate III
December 10, 2015
Question

Unsuccessful entering in sleep mode and wait for interrupt for wakeup

  • December 10, 2015
  • 1 reply
  • 726 views
Posted on December 10, 2015 at 14:50

Dear all,

I am using a STM32F103VEH micro-processor. I intend to put the processor into sleep mode and configure it so it will wake up by receiving any interrupt. I use the following code:

  uint32_t tmpreg = 0;

  tmpreg = PWR->CR;

  tmpreg &= CR_DS_MASK;

  tmpreg |= PWR_Regulator_LowPower;

  PWR->CR = tmpreg;

  // Ask the processor to sleep now.

  SCB->SCR &= ~(SCB_SCR_SLEEPONEXIT | SCB_SCR_SLEEPDEEP);

  // Wait for any interrupt to wake up.

  __WFI();

When a packet is received over UART and interrupt is triggered so I expect the processor to just operate normally, but the system will be just frozen when I run the code. When I remove ''__WFI()'' the system is not frozen anymore but I guess I need to have this command to wait for an interrupt to wake the processor up after a sleep.

Does anybody kno if I am doing anything wrong to put the processor into sleep mode and the expect it to be waken up when an interrupt is triggered?

Regards,

Dan

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    December 10, 2015
    Posted on December 10, 2015 at 17:23

    Make sure the PWR/BKP domain clocks are enabled, and unlocked.

    Review how the library does it, at a glance clearing the bits isn't how they do it.

    void PWR_EnterSTOPMode(uint32_t PWR_Regulator, uint8_t PWR_STOPEntry)
    {
    uint32_t tmpreg = 0;
    /* Check the parameters */
    assert_param(IS_PWR_REGULATOR(PWR_Regulator));
    assert_param(IS_PWR_STOP_ENTRY(PWR_STOPEntry));
    /* Select the regulator state in STOP mode ---------------------------------*/
    tmpreg = PWR->CR;
    /* Clear PDDS and LPDS bits */
    tmpreg &= CR_DS_MASK;
    /* Set LPDS bit according to PWR_Regulator value */
    tmpreg |= PWR_Regulator;
    /* Store the new value */
    PWR->CR = tmpreg;
    /* Set SLEEPDEEP bit of Cortex System Control Register */
    SCB->SCR |= SCB_SCR_SLEEPDEEP;
    /* Select STOP mode entry --------------------------------------------------*/
    if(PWR_STOPEntry == PWR_STOPEntry_WFI)
    {
    /* Request Wait For Interrupt */
    __WFI();
    }
    else
    {
    /* Request Wait For Event */
    __WFE();
    }
    /* Reset SLEEPDEEP bit of Cortex System Control Register */
    SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP);
    }

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..