Question
Typo in STM32F030
Posted on March 16, 2017 at 16:05
I found a typo in the interrupt vector table of the STM32F030 & STM070 Reference Manual RM0360 Rev 3.
On page 172, an additional 'Reserved' line is inserted at position 19. Also, the address given for the 'Reserved' line in position 18 is given as 0x0000 0084 when it should be 0x0000 0088.
I'm not sure if this is the best place to send this type of information, but it's where I'm starting.