Skip to main content
darius
Associate
October 18, 2016
Question

Trouble with internal flash, EEPROM emulation

  • October 18, 2016
  • 2 replies
  • 669 views
Posted on October 18, 2016 at 09:51

Hello,

i have problem with eeprom, then i erasing eeprom (writing 0 or any other values) then everything is working without problem , later then i write 0 then everything is working fine, but if i write other value then i got error 2, please help,

i am suing STM32F103RB

i provided test code:

#include <EEPROM.h>

byte ReadStatus ;

uint32 as;

 int as1 = 0;

void setup() {

  Serial.begin(115200);

  delay(5000);

  uint32 *mem = (uint32 *)0x08019000 + 1010;

  as = *mem & 0xFFFF;

  if (as != 0) { // if value is not zero then erase memory

    FLASH_Unlock();

    for (int i = 0 ; i < 2040 ; i++ ) {

      ReadStatus = FLASH_ProgramHalfWord(0x08019000 + (i * 4), 0);

      Serial.println(ReadStatus);

    }

    FLASH_Lock();

  }

  for (int i = 0 ; i < 2040 ; i++ ) {  // debug - check erased memory

    uint32 *mem = (uint32 *)0x08019000 + i;

    as = *mem & 0xFFFF;

    Serial.print(*mem); Serial.print(''-''); Serial.println(as);

    delay(1);

  }

  delay(5000);

}

void loop() {

  ReadStatus = FLASH_WaitForLastOperation(1000);

  Serial.print(String(ReadStatus)); Serial.print(''-'');

  FLASH_Unlock();

  ReadStatus = FLASH_ProgramHalfWord(0x08019000 + 4, as1); // there i got error code 2

  FLASH_Lock();

  Serial.print(String(ReadStatus)); Serial.println(''-'');

  as1++;

  delay(5000);

}
    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    October 18, 2016
    Posted on October 18, 2016 at 10:08

    FLASH is not erased by writing zeros into it.

    The library you are using will probably provide a function like FLASH_EraseSector() to erase a sector in FLASH. Check your library's documentation and RM0008.

    JW
    darius
    dariusAuthor
    Associate
    October 18, 2016
    Posted on October 18, 2016 at 10:20

    you are right, there is not erasing, just writing zeros, but where is the problem ? in first step after code upload then i writing to memory any values (from 0 to 65535) then everything work fine, later then i need to write some value in memory except 0 then i got error !?

    i cant find out why i can write anything after first startup after code upload, and why i cant write later !?