Question
Timer2 Configuration
Posted on May 15, 2017 at 10:47
I'm working on STM32 nucleo432lkc. I'm trying to divide the MSI frequency for the timer by 50 but when I try this , i get nothing on the ouput of the pin. Below is the timer 2 code :
void TIM2_init(void)
{TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_MasterConfigTypeDef sMasterConfig;__TIM2_CLK_ENABLE();
TIM_init_struct.Instance = TIM2; TIM_init_struct.Init.Prescaler = 0 ;//40000; TIM_init_struct.Init.CounterMode = TIM_COUNTERMODE_UP; TIM_init_struct.Init.Period = 0 ;//491; TIM_init_struct.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; TIM_init_struct.Init.RepetitionCounter = 0;//HAL_TIM_Base_Init(&TIM_init_struct);
if(HAL_TIM_Base_Init(&TIM_init_struct)== HAL_OK) { /* Start the TIM time Base generation in interrupt mode */ HAL_TIM_Base_Start_IT(&TIM_init_struct); } HAL_NVIC_SetPriority(TIM2_IRQn, 0, 1); HAL_NVIC_EnableIRQ(TIM2_IRQn); sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&TIM_init_struct, &sClockSourceConfig) != HAL_OK) { TIM_Error_Handler(); }sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&TIM_init_struct, &sMasterConfig) != HAL_OK) { TIM_Error_Handler(); }}void TIM2_IRQHandler()
{//}
HAL_TIM_IRQHandler(&TIM_init_struct);}
#include 'stdbool.h'bool test = false;void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){ int timerValue = HAL_RCC_GetSysClockFreq(); if (test) { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET); test = false; } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET); test = true; }// HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0); HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_3);}