Question
TIM1 update interrupt not firing.
Posted on September 11, 2015 at 13:11
Hello Everybody.
I am having trouble with the output compare function of an STM32F401RE. I am testing the OC function to generate a waveform by toggling an output at the compare point and the overflow point.The counter is running and comparing correctly, but I cannot get the interrupt to fire for the update event when the counter overflows.I have a break point in the interrupt routines, but the update event (for overflow) never occours.The flag is being set in TIM1_SR bit 0 (UIF: Update interrupt flag), but the interrupt is not called.My code (generated through STM32CubeMX - this is the first time I have used this program, so may be missing something with the new abstration layer!) is below.I hope someone can help, than kyou in advance!int main(void){ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* interrupt enables */ /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM1_Init(); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1){}}/*** @brief This function handles TIM1 update interrupt and TIM10 global interrupt. - timer overflow*/void TIM1_UP_TIM10_IRQHandler(void){ HAL_TIM_IRQHandler(&htim1); /* clears flags etc... */}/*** @brief This function handles TIM1 capture compare interrupt.*/void TIM1_CC_IRQHandler(void){ HAL_TIM_IRQHandler(&htim1); /* clears flags etc... */}/** System Clock Configuration*/void SystemClock_Config(void){ RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; __PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 16; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4; RCC_OscInitStruct.PLL.PLLQ = 7; HAL_RCC_OscConfig(&RCC_OscInitStruct); RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2); HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);}/* TIM1 init function */void MX_TIM1_Init(void){ TIM_MasterConfigTypeDef sMasterConfig; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig; TIM_OC_InitTypeDef sConfigOC; __TIM1_CLK_ENABLE(); TIM1->DIER = 0x0002; /* initialise basic timer operation */ htim1.Instance = TIM1; htim1.Init.Prescaler = 0; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 0x0fff; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; HAL_TIM_OC_Init(&htim1); sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig); sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE; sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE; sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF; sBreakDeadTimeConfig.DeadTime = 0; sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE; sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH; sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE; HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig); /* configure the timer to run with output compare */ sConfigOC.OCMode = TIM_OCMODE_TIMING; //sConfigOC.OCMode = TIM_OCMODE_INACTIVE; sConfigOC.Pulse = 0x00ff; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET; sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET; HAL_TIM_OC_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1); /* start the output compare module */ HAL_TIM_Base_Start(&htim1); HAL_TIM_OC_Start(&htim1, TIM_CHANNEL_1); }void HAL_MspInit(void){ HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0); /* System interrupt init*/ /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}void HAL_TIM_OC_MspInit(TIM_HandleTypeDef* htim_oc){ if(htim_oc->Instance==TIM1) { /* Peripheral clock enable */ //__TIM1_CLK_ENABLE(); DOES NOT WORK HERE! moved to MX_TIM1_Init() /* Peripheral interrupt init*/ HAL_NVIC_SetPriority(TIM1_UP_TIM10_IRQn, 0, 0); HAL_NVIC_EnableIRQ(TIM1_UP_TIM10_IRQn); HAL_NVIC_SetPriority(TIM1_CC_IRQn, 1, 0); HAL_NVIC_EnableIRQ(TIM1_CC_IRQn); }}