systick is not working after jump.
below are the codes(0x0801E000U) which is used for jump:
#define PROJ1_FLASHADDR 0x08000000U
#define PROJ2_FLASHADDR 0x0801E000U
__disable_irq();
/* Get the main application start address */
uint32_t jump_address = *(__IO uint32_t *)(PROJ1_FLASHADDR + 4);
/* Set the main stack pointer to to the application start address */
__set_MSP(*(__IO uint32_t *)PROJ1_FLASHADDR);
/* Create function pointer for the main application*/
void (*pmain_app)(void) = (void (*)(void))(jump_address);
/* Now jump to the main application*/
pmain_app();
i am also enabling irq in the beginning of main function.