STM32L496 embedded bootloader CAN interface not working
I'm using the STM32L496 and attempting to get the CAN communication working with the embedded bootloader. I can put the device into boot mode, but as soon as I send a CAN frame (0x79 Identifier, or any frame for that matter) the device seems to jump to or reset to the main application code. I would expect it to go into the bootloader where I can send the bootloader CAN commands. I have a 24MHz oscillator connected to the HSE pins.