STM32L4 SMBus example code
Hello All,
I want to use the SMBus library written by MCD team. Could you please help me out with sample code to communicate with two microcontrollers?
Here is the snippet of my code:
/* SCL */
GPIO_InitStruct.Pin = GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_OD; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_I2C1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_2);
HAL_NVIC_SetPriority(I2C3_ER_IRQn, 0, 2); HAL_NVIC_EnableIRQ(I2C3_ER_IRQn); HAL_NVIC_SetPriority(I2C3_EV_IRQn, 0, 1); HAL_NVIC_EnableIRQ(I2C3_EV_IRQn);SMBus_Handle.Instance = I2C3;
SMBus_Handle.Init.Timing = ((uint32_t)0x1042C3C7); // for 10KHz SMBus_Handle.Init.AnalogFilter = SMBUS_ANALOGFILTER_ENABLE; SMBus_Handle.Init.OwnAddress1 = 0x55; SMBus_Handle.Init.AddressingMode = SMBUS_ADDRESSINGMODE_7BIT; SMBus_Handle.Init.DualAddressMode = SMBUS_DUALADDRESS_DISABLED; SMBus_Handle.Init.OwnAddress2 = 0; SMBus_Handle.Init.OwnAddress2Masks = SMBUS_OA2_NOMASK; SMBus_Handle.Init.GeneralCallMode = SMBUS_GENERALCALL_DISABLED; SMBus_Handle.Init.NoStretchMode = SMBUS_NOSTRETCH_DISABLED; SMBus_Handle.Init.PacketErrorCheckMode = SMBUS_PEC_DISABLED;#ifdef SLAVE_MODE
SMBus_Handle.Init.PeripheralMode = SMBUS_PERIPHERAL_MODE_SMBUS_SLAVE;#elif defined MASTER_MODE SMBus_Handle.Init.PeripheralMode = SMBUS_PERIPHERAL_MODE_SMBUS_HOST;#endif SMBus_Handle.Init.SMBusTimeout = SMBUS_TIMEOUT_DEFAULT;HAL_SMBUS_Init(&SMBus_Handle);
Main code :
HAL_SMBUS_Master_Transmit_IT(&SMBus_Handle,SLAVE_DEVICE_ADDRESS,Master_Data,sizeof(Master_Data),SMBUS_AUTOEND_MODE);
while( HAL_SMBUS_GetState(&
SMBus_Handle
) != HAL_SMBUS_STATE_READY);if(Flag_In_Tx_ISR == true)
{ // transfer completedFlag_In_Tx_ISR
= false; }// expecting some string from slave receiver
HAL_SMBUS_Master_Receive_IT(&SMBus_Handle,SLAVE_DEVICE_ADDRESS,(uint8_t*)Buffer,sizeof(Slave_Data),SMBUS_AUTOEND_MODE);
while( HAL_SMBUS_GetState(&
SMBus_Handle
) != HAL_SMBUS_STATE_READY);if(Flag_In_Rx_ISR == true)
{// receive the string and do something
Flag_In_Rx_ISR
= false; }I have just added snippet of code... just let me know if anything is wrong in this code.
Thanks,
Nikhil