Question
STM32L temperature trimming values 90° or 110°
Posted on October 10, 2012 at 09:25
Hello,
currently I'm evaluating the internal temperature senor of the STM32L151, but in the docs are different values for trimming values given. Sometimes 90° is stated somtimes 110°, so which value is correct? STM32L151xx datasheet -> 110° for upper factory trimming value STM32L151xx errata -> 90° RM0038 reference manual -> 90° regards thomas